Camera Selector

Easy connection for your microscopy imaging project

Use our cameras with our open source µManager plugin!

Discover

Last-Time Buy and Last-Time Delivery for Sony CCD-based cameras

Migrate to CMOS or stay with CCD?
We support you in finding the best option for your project.

Learn more

Kudan and Allied Vision

A new exciting collaboration between Kudan and Allied Vision. The Kudan Grand SLAM software will now support the Nerian Ruby 3D depth camera and is available as part of Kudan’s Mobile Robot Development Kit for Autonomous Mobile Robots.

Learn more

High-resolution short-wave infrared cameras

Coming soon: 
Alvium SWIR cameras with Sony IMX992 and IMX993

Learn more 

Discover the Goldeye XSWIR Cameras

Goldeye XSWIR cameras with extended SWIR sensitivity up tp 2.2 µm and integrated dual-stage cooling (TEC2). 
Learn more about the award-winning Goldeye XSWIR cameras and XSWIR sensor technologies 


Find out more

Choose the right camera for your application

Go to camera selector

Take your career to the next level!

Allied Vision is looking for people like you. We are always on the lookout for ambitious professionals who share our passion for quality and innovation and who like to make our customers happy.

Find out more

Focus on what counts

We don't just develop cameras. We provide answers.

At Allied Vision, we help people achieve their goals with digital cameras for computer vision. This technology opens up a range of new possibilities for businesses throughout a broad spectrum of industries. Originally built with the needs of manufacturers in mind, our camera portfolio now extends to a wide variety of sectors including science and research, medical imaging, traffic monitoring, and sports analytics.

Given the wide variety of application challenges our customers face, we have always endeavored to offer a flexible and variable camera portfolio. This is why we design our cameras to be modular. The result is a diversity of sensors, lens mounts, filters, board-level versions, and many more options that maximize flexibility.

Discover more about Allied Vision

The image you need

Camera technology for your requirements

Our engineers design digital cameras with a large scope of resolutions, frame rates, bandwidths, interfaces, spectral sensitivities, sensor technologies, and technical platforms. We have created a modular concept to ensure that your camera adapts to requirements of your application and not the other way around.

We know how to help you find the best camera solution for your application. That includes a digital camera, but also the right lens, the right connectivity hardware and the right software interface. Our job is to reliably deliver the image you need, when you need it and how you need it.

 

Learn more about our pRODUCTS

From embedded to scientific

Vision solutions for your application

Do you need help

Technical information and support

Allied Vision is at your side throughout the life cycle of your image-processing project. We are here to help you integrate your camera into your system, solve software issues and ensure your system performs as it should even years after you purchased your camera.

Our specialists provide expert advice, engineering, manufacturing and support for digital cameras, their peripherals and their integration into your machine vision system.

Get an overview of helpful information and downloads!

Stay tuned!

Latest news

Alvium camera lens mounts

Product News

Allied Vision offers three lens mount options for Alvium cameras. Discover more about these mounts.

What are the differences between S-Mount, CS-Mount, and C-Mount and the benefits of each mount?

One of your first decisions when selecting a camera for your vision system is deciding on the lens mount. But what are the differences between C-Mount, CS-Mount, and S-Mount. What are the benefits of one lens mount versus another lens mount. Either way, you need a lens mount to attach the lens to the camera. Regardless of the lens mount, every Alvium camera offers the same highly accurate sensor alignment to create crisp images even at the edges.
All three lens mounts are screw-style lens mounts and offer a secure lens connection to the camera. Although with S-Mount, you must use a locking nut to secure the lens to the mount.

 

C-Mount

So lets start with C-Mount. C-Mount is the most popular lens mount in the machine vision ecosystem. One of the main benefits of this is that there is a very wide range of lenses, filters, and other accessories available. It's easy to find a lens with specific characteristics to match your vision application needs. There is also a lot of new lens technology options in C-Mount lenses including new liquid lens which provide quick autofocus.

C-Mount is suitable for sensors up to Type 1.3 or 24 mm diagonal (so any Alvium model).
C-Mount lenses are designed for machine vision and are often more robust compared to S-Mount and CS-Mount. Many lenses have a wide temperature range or enhanced shock and vibration tolerances. Although there are C-Mount to S-Mount adapters on the market, there is a limited range of compatible lenses.

 

S-Mount

S-Mount is a popular lens mount in embedded vision systems due to its very compact form-factor and inexpensive (good value) lenses. Due to its small size, it is only suitable for sensors up to Type 2/3, although this is also lens dependent. With larger sensors, you will experience vignetting around the edges of the image.

With  C-Mount and CS-Mount lenses, you just need to confirm the mount type, the sensor format, and the megapixel rating to get an image. For S-Mount, you need additional tests to check where the lens is in the camera body when focused at the object. The lens may protrude too much or not at all. This may be an issue when using a locking nut to fix the lens in place.

 

CS-Mount

What about CS-Mount? Historically CS-Mount was a popular lens mount security applications but less so in machine vision applications. From a form-factor stance, CS-Mount lenses are 5mm shorter, meaning that the lens is closer to the image sensor. It is possible to use a C-Mount or S-Mount lens with CS-Mount provided you use the appropriate lens adapter. Although many lenses allow you to set the focus, you can't always adjust the iris. CS-Mount lenses are often mass produced and provide decent quality for the price. It is possible to find higher quality lenses which use aspherical lens technology.


Still confused about which lens mount to select? Contact us today to discuss your vision application and requirements and one of our vision experts can help you figure out which lens mount, lens, filter, or other camera accessories are right for your application.

Contact us