eGrabber Memento
Event Logging Tool
- Accurate logging of events related to the camera, the frame grabber and its driver as well as the host application
- Graphical representation of time-stamped events on a precise timeline with context information
- Logic analyzer feature to help users analyze selected system events
- Support for setting up, debugging and profiling the system
- Availability with all Coaxlink and Grablink cards in the PC
- Non-intrusive tool requiring low CPU usage
- Compatible with Windows, Linux, and macOS
Description
In high-end inspection machines using vision, the frame grabber is responsible for acquiring images in synchronization with numerous external devices such as motion or lighting controllers, not to mention the camera itself. Debugging these systems often requires complex equipment, for example, oscilloscopes and logic analyzer, which are used along with software profilers. The problem is even more acute with the latest cameras available, which allow for very fast frame rates exceeding several hundred, even thousand frames per second.
eGrabber Memento has been designed to simplify that process. During the operation, Memento records a very detailed log of events related to the camera, the frame grabber and its driver, as well as the host application.
Download Area
Release Notes
eGrabber Memento 26.04
Setup Files (Current version 26.04.1)