Deep Learning Bundle
Convolutional Neural Network-Based Inspection Libraries
- Set of Deep Learning inspection libraries
- Optimized for machine vision applications
- Performs image classification, supervised or unsupervised segmentation and object localization
- Simple API
- Free Deep Learning Studio application for dataset creation, training and evaluation
- Supports data augmentation and masks
- Compatible with CPU and GPU processing
Why Choose Open eVision’s Deep Learning Bundle?
Deep Learning Bundle has been tailored, parametrized and optimized for analyzing images, particularly for machine vision applications.
Deep Learning Bundle has a simple API and the user can benefit from the power of deep learning technologies with only a few lines of code.
Try before you buy: Deep Learning Bundle comes with the free Deep Learning Studio training and evaluation application.
Deep Learning Bundle Feature Comparison
EasyClassify, EasySegment and EasyLocate can be purchased as part of the Deep Learning bundle or individually as inference only licenses.
Main Benefits
What Is Deep Learning?
Neural Networks are computing systems inspired by the biological neural networks that constitute the human brain. Convolutional Neural Networks (CNN) are a class of deep, feed-forward artificial neural networks, most commonly applied to analyzing images. Deep Learning uses large CNNs to solve complex problems difficult or impossible to solve with so-called conventional computer vision algorithms. Deep Learning algorithms may be easier to use as they typically learn by example. They do not require the user to figure out how to classify or inspect parts. Instead, in an initial training phase, they learn just by being shown many images of the parts to be inspected. After successful training, they can be used to classify parts, or detect and segment defects.
Open eVision Deep Learning Studio
Open eVision includes the free Deep Learning Studio application. This application assists the user during the creation of the dataset as well as the training and testing of the deep learning tool. For EasySegment, Deep Learning Studio integrates an annotation tool and can transform prediction into ground truth annotation. It also allows to graphically configure the tool to fit performance requirements. For example, after training, one can choose a tradeoff between a better defect detection rate or a better good detection rate.
Performance
Deep Learning generally requires significant amounts of processing power, especially during the learning phase. Deep Learning Bundle supports standard CPUs and automatically detects Nvidia CUDA-compatible GPUs in the PC. Using a single GPU typically accelerates the learning and the processing phases by a factor of 100.
Other Benefits
Neo Licensing System
Neo is the new Licensing System. It is reliable, state-of-the-art, and is now available to store Open eVision and eGrabber licenses. Neo allows you to choose where to activate your licenses, either on a Neo Dongle or in a Neo Software Container. You buy a license, you decide later.
Neo Dongles offer a sturdy hardware and provide the flexibility to be transferred from a computer to another. Neo Software Containers do not need any dedicated hardware, and instead are linked to the computer on which they have been activated.
Neo ships with its own, dedicated Neo License Manager which comes in two flavours: an intuitive, easy to use, Graphical User Interface and a Command Line Interface that allows for easy automation of Neo licensing procedures.
All eVision Libraries For Windows And Linux
- Microsoft Windows 11, 10 for x86-64 (64-bit) processor architecture
- Microsoft Windows 11, 10 IoT Enterprise on x86_64 systems
- Linux for x86-64 (64-bit) and ARMv8-A (64-bit) processor architectures with a glibc version greater or equal to 2.18