Use Vimba instead of Universal Package for MATLAB
Vimba is our future-proof SDK for all current Allied Vision cameras with GigE Vision and FireWire (IEEE 1394) interface, whereas the Universal Package is a legacy SDK that is no longer recommended for use with MATLAB.
- Uninstall the Universal Package (or at least unregister the AVT Adaptor for MATLAB).
- Download Vimba from: www.alliedvision.com/en/products/software.html
- Install Vimba (do not deselect the transport layers).
- Use Vimba's GenTL-compliant transport layer with MATLAB 2012b (or higher), which provides the 'gentl' Adaptor to access the GenTL transport layers. Do not use the GenICam_VC80_i86_v_2_3_0 driver from MathWorks.
Starting with version R2014a, MATLAB requires to install the Support Package for GenICam GenTL Interface.
Note:
The MATLAB Adaptor uses the UniAPI proprietary feature names, whereas Vimba's GenTL uses the GenICam standard feature names for GigE and FireWire cameras. Please consider these differences.
Back to list