Integrating Allied Vision cameras into NI LabVIEW and other National Instruments (NI) software

To integrate Allied Vision IEEE 1394, USB 3.0, or GigE cameras into NI software, the IMAQdx driver is necessary.
The configuration is described on the NI website at:


The NI IMAQdx driver must be purchased from National Instruments and can be downloaded as an evaluation version at: sine.ni.com/nips/cds/view/p/lang/en/nid/12892

After installation of the package, the cameras can be used with any NI software (LabVIEW, Vision Builder...).

For LabVIEW resources, please refer to the NI website, manuals, and support resources. See also the very active and helpful NI Machine Vision Forum at: forums.ni.com/t5/Machine-Vision/bd-p/200



Back to list