Partner firmware downloads
Hi partners! Here you can find previous firmware downloads for Allied Vision cameras, with summarized change logs.
Guppy PRO
Guppy PRO firmware V2012-Oct-10
30.10.2012 - Reason for the firmware update:
Bug fixes:
#GUPPYPRO-31 / GUPPYPRO-37 / GUPPYPRO-38:
After soft reset camera could change color
#GUPPYPRO-11 / GUPPYPRO-48:
First one-shot command might not be executed
#Fix to improve update / boot reliability
Version of the firmware files:
Guppy PRO F-031B/C, Guppy PRO F-032B/C, Guppy PRO F-033B, Guppy PRO F-046B, Guppy PRO F-095C, Guppy PRO F-125B/C, Guppy PRO F-146B/C, Guppy PRO F-201B/C, Guppy PRO F-503B/C
Firmware 00.01.00.10:
µC version 00.01.06.09
FPGA version 00.01.00.10
Guppy PRO F-033C, Guppy PRO F-046C
Firmware 00.01.00.11:
µC version 00.01.06.09
FPGA version 00.01.00.11
Please see the release notes in the packages for more information.
Manta
18.01.2013 - Reason for the firmware update:
- Fixed StreamBytesPerSecond calculation issues for all Manta cameras (GEV-59)
- Fixed LUTControl parameters (e.g., LUTEnable, LUTMode) not saved in ConfigFile for all Manta cameras (GEV-263)
- Fixed: changed Gain or Offset could lower maximum gray level, only Manta G-032(GEV-283)
The new firmware is part of the Manta Firmware loader, version 00.01.44.09. This loader support the following Manta models:
G-031B/C, G-032B/C, G-033B/C, G-046B/C, G-095C, G-125B/C, G-145B/C, G-145B/C-30, G-145B NIR, G-146B/C, G-201B/C, G-201B/C-30, G-504B/C
Please see the release notes in the packages for more information.
26.10.2012 - Reason for the firmware update:
Improved production yield for Manta G-032B/C and Manta G-095C (GEV-217)
The new firmware is part of Manta Firmware loader 00.01.44.08:
New versions in this loader:
MG032B/C: 00.01.44.08
MG095C: 00.01.44.08
For all other Mantas, the following versions remain:
MG031B/C: 00.01.44.05
MG033B/C: 00.01.44.04
MG046B/C: 00.01.44.04
MG125B/C: 00.01.44.04
MG145B/C: 00.01.44.04
MG145B/C-30: 00.01.44.04
MG145BNIR: 00.01.44.06
MG146B/C: 00.01.44.04
MG201B/C: 00.01.44.04
MG201B/C-30: 00.01.44.04
MG504B/C: 00.01.44.04
Please see the release notes in the packages for more information.
Marlin
05.11.2010 - Reason for firmware update:
All cameras with serial numbers, beginning with 6xxxxxxxx have a revised hardware together with new firmware versions. These cameras do have the newest Firmware.
For older cameras we have a Package with the newest firmware revisions.
Any mixing of hardware and firmware other than listed in the firmware release note, may result in a non-functional or even defective camera which is explicitly excluded from the guarantee.
Marlin F-131B firmware V00.03.00.00
15.11.2010 - Reason for Firmware Update:
- Micro Controller AT91 Rev S is dicontinued.
- Micro Controller AT91 Rev SB needs to be implemented.
This revision requires a revised boot loader.
What changes?
a) AT91 rev S --> AT91 rev SB
b) new boot loader with new firmware
Revision information:
- Package: 00.03.00.0
- FPGA: 00.01.00.00
- uC: 3.50
- BL: 2.5
Bug fixes:
#415/#420/#640: "saving data to flash" may lead to "Profile doesn't exist." #359: Storing of usersets may lead to errors
If you have any question, please contact Support.
Pike
23.02.2012 - Reason for firmware update:
#748 – Corrected: Soft Reset feature didn’t reset the camera due to wrong internal handling of the feature
#928 / #1030 - Corrected: Write settings from xml-file into the camera sometimes failed and initialization sometimes failed (also in some third party applications as e.g. CMU 1394 driver).
Please see the release notes in the packages for more information.
Pike F-1600 firmware upgrade V201105
30.05.2011 - Reason for firmware update:
New Defect Pixel Correction feature
Pike F-1100 firmware upgrade V201105
30.05.2011 - Reason for firmware update:
New Defect Pixel Correction feature
21.12.2009 - Reason for firmware update:
#739 - Pike stability service pack
Pike F-210c firmware V00.03.02.00
28.04.2009 - Reason for firmware update:
#572 - Revised Subsampling Mode (no speed increase anymore)
Stingray
Stingray F-504b/c V00.03.02.00
09.04.2014 - Reason for firmware update:
Bug fixes:
#FIREWIRE-62: One push operation was interrupted after the first automatically taken image, if the newly computed shutter value
- was below the lower value of auto shutter range or
- was above the upper value of auto shutter range
Ensured one push shutter/gain start within ranges.
Stingray firmware update V03.01.00
13.02.2012 - Reason for the firmware update:
#677: Stingray Defect Pixel Correction didn’t detect defects
#768: Sequence mode didn't work after after Multishot Mode was used
#824: Quick Format Change Mode didn’t work reliable
#835: No acknowledge error when opening camera, after closing it with Auto Gain or Auto Shutter enabled
#846: Stingray disappeared from bus when opening, after closing it with Auto Shutter enabled
#1032: Using YUV422 and RGB for color interpolation showed one invalid column
#1036: Combination of One-Push /Auto Shutter and White balance may not work parallel and inhibit each other
Please see the release notes in the packages for more information.
Stingray F-504b/c firmware V00.03.00.01
21.04.2010 - Reason for firmware update:
Fixed Bugs
- #875: Stingray defect pixel correction does not detect defects
- #876: Stingray Defect pixel correction has no influence in binning mode
Stingray firmware update V2010-August
04.08.2010 - Reason for the firmware update:
The recent firmware suffered from a bug, which has been solved now.
Solved bug:
- #798: Wrong gain settings after initialize
Stingray firmware update V2010-June
21.06.2010 - Reason for firmware update:
The recent firmware suffered from a few bugs, which have been solved now.
Solved bugs:
- #774 randomly broken images (free run and triggered mode)
- #771 format changes in sequence mode don´t work
- #562 wrong Exposure Offset at 0xF1000208 TIMEBASE register
Stingray F-145b/c firmware update V2021-April
26.03.2010 - Reason for firmware update:
In dedicated combinations, the sequence mode did not work properly (#771)
Legacy firmware
This legacy firmware is provided for Allied Vision distribution partners only. If you are not an official Allied Vision distribution partner, we strongly recommend that you contact our technical support before loading a new firmware on your camera.