=========================================================================== AVT NeuroCheck Interface - Release Notes Version: 4.0.0 Date: February 2, 2012 Document version: 1.0.1 Date: July 29, 2015 =========================================================================== -------------------------------- Components and Version Reference -------------------------------- The AVT NeuroCheck Interface v4.0 can be used with NeuroCheck® v6.0 (Service Pack 3 or later). It consists of the following components: - AVT Interface DLL AVTNcUni.NET.dll 4.0.3 - Camera Configuration DLL AVTCameraControl.dll 1.2.0 --------------------- Hardware Requirements --------------------- PC or laptop with 1 GHz 32-bit (x86) or 64-bit (x64) processor or better. For further hardware requirements please refer to the AVT Universal Package release notes and the NeuroCheck® documentation. --------------------------- Supported Operating Systems --------------------------- The AVT NeuroCheck Interface is designed for the 32-bit and 64-bit Windows operating systems: Windows 7, Vista, and XP --------------------- Software Requirements --------------------- Before installing the AVT NeuroCheck Interface please make sure that the following software packages are installed: - NeuroCheck® version 6.0 (SP3 or later) - AVT Universal Package version 2.0 or later Please note: The AVT Universal Package can be downloaded free of charge under: http://www.alliedvisiontec.com/us/products/software/windows/avt-universal-package.html For further information about the AVT Universal Package and its requirements please refer to the corresponding release notes. ------------ Installation ------------ To install the AVT NeuroCheck Interface simply start the installer executable (AVTNeuroCheckInterface_4v0.exe) and follow the instructions shown on the screen. ----------------------------------------------- Setting camera parameters from a check function ----------------------------------------------- Timeout for image acquisition: To ensure proper error handling a timeout is used inside the AVT NeuroCheck Interface to monitor the image acquisition. Therefore the check function 'Capture image' returns after an image is received or the timeout is exceeded. The check function 'Control Device' can be used to change the parameter 'Timeout' dynamically. The default value is 2 seconds. Please keep this in mind when using triggers or long exposure times. ------------------- Current Limitations ------------------- Currently it is not possible to change other camera settings during operation. ------------------------------------------ Contacting Allied Vision Technologies GmbH ------------------------------------------ Allied Vision Technologies GmbH Taschenweg 2a 07646 Stadtroda Germany www.alliedvisiontec.com ------------------------------ AVT Technical Software Support ------------------------------ You can reach AVT’s Application Engineering Team via the corresponding contact form for your region: Asia Pacific ------------ http://www.alliedvisiontec.com/apac/support/contact-support.html Europe, Middle East and Africa ------------------------------ http://www.alliedvisiontec.com/emea/support/contact-support.html Germany ------- http://www.alliedvisiontec.com/de/support/support-kontaktieren.html The Americas ------------ http://www.alliedvisiontec.com/us/support/contact-support.html