Universal Package logging and troubleshooting (UniAPI, UniControl)
Logging:
In order to write all calls and return codes to UniControl.log (for example, C:\WINDOWS\system32), copy the UniControl.ini file into the directory where UniControl.dll is loaded.
Since the logging decreases the performance, use it only for debugging.
Troubleshooting:
UniAPI supports AVT cameras loading interface-specific core libraries. For troubleshooting the camera behavior, these APIs and viewer applications could be helpful:
Interface | API | Viewer | Package |
1394 DCAM | FireGrab | GrabDemo.exe | FirePackage |
GigE Vision | PvAPI | SampleViewer.exe | GigE Sample Viewer |
Back to list