GigE camera disconnects all the time
If your GigE camera disconnects all the time although all NIC and camera settings are correct and you get the error code -3 VmbErrorNotFound (Vimba) or error code 6 ePvErrNotFound (PvAPI), there are two possible solutions:
- The firewall may cause the issue. In that case, please disable it.
- Make sure that all other NICs are not connected or have a valid IP address in a different subnet than the camera NIC. An IP conflict may also lead to permanent disconnection scenarios.
Back to list