Level Trigger Mode with GigE Vision / GenICam features
To set up the external Level Trigger Mode with GigE Vision / GenICam features, use the following settings:
Acquisition->Trigger->TriggerSelector = FrameStart
Acquisition->Trigger->TriggerMode = On
Acquisition->Trigger->TriggerSource = Line1 (or another input)
Acquisition->Trigger->TriggerActivation = LevelHigh (or LevelLow for reverse polarity)
Controls->Exposure->ExposureAuto = other (or, depending on the camera model: ExposureMode = TriggerWidth)
Vimba Viewer users: The Trigger IO tab enables easy configuration.
Back to list