Archive

Allied Vision Technologies to Premiere Array of New Cameras at the AIA Vision Show in Boston

New Prosilica GT model with CMOSIS sensor, expanded Manta range and new Bigeye camera model with active cooling.

From May 8-10, 2012 Allied Vision Technologies (AVT) will be exhibiting at the AIA Vision Show in Boston, Massachusetts, North America’s leading machine vision show where AVT will be premiering a number of new cameras at booth #323.

Prosilica GT: New CMOSIS and High Resolution Models
The Prosilica GT cameras by Allied Vision Technologies are Gigabit Ethernet cameras designed to perform in extreme environments. Able to work in temperatures from -20⁰ C to 60⁰C and varying light conditions, the Prosilica GT cameras feature auto-iris (P-iris and DC), PoE (Power over Ethernet) and PTP IEEE1588, a function that manages clock synchronization of multiple devices across an Ethernet network. The Prosilica GT cameras are well-suited for a wide variety of demanding  machine vision, industrial and outdoor imaging applications.

Three new cameras from the Prosilica GT family will make their debut at THE Vision Show:  The 2 Megapixel Prosilica GT2000 with the fast and highly sensitive CMOSIS CMV-2000 sensor, the 8 Megapixel Prosilica GT3000 featuring the quad-tap Kodak-KAI-08050 progressive scan CCD sensor and the 29 Megapixel Prosilica GT6600 with the 35mm format Kodak KAI-29050 sensor.


Manta: New EXview HAD II CCD Models
The Manta family of feature-rich GigE Vision cameras welcomes three new cameras, Manta G-282, G-283 and G-609, featuring second generation Sony EXview HAD CCD dual-tap sensors that combine high resolution and fast frame rates, which provide excellent sensitivity and image quality. The 5 Megapixel dual-tap Manta G-505 will also make its debut at THE Vision Show.

The Manta cameras offer an outstanding price/performance ratio as well as many modular options such as PoE (Power over Ethernet), angled head variant, and/or sensor variants, and a robust housing to fit into any applications.

Bigeye: Long Exposure with Peltier Cooling
The new Bigeye G-283B is a low-noise CCD monochrome camera that offers excellent image quality thanks to its 2.8 Megapixel Sony ICX674 EXview HAD CCD II sensor. It features a Peltier cooling device for a superior signal-to-noise ratio even with long exposure times. The Bigeye is ideal for industrial and scientific imaging applications and non-destructive evaluation of photo-sensitive objects.