Mako Camera Powers Audi Mind Race

The Audi Mind Race is a technological challenge, which features Audi R18 e-tron (1:24) miniature cars, which FC Barcelona players moved through their own mind, as the energy generated by the players' brains powered the vehicles.

A vision system using a Mako G-223B camera by Allied Vision Technologies gathered and analyzed image data to produce real-time statistics and audio-visual effects that were projected onto the circuit.

The Mako G-223B camera with Gigabit Ethernet interface was provided by Infaimon, AVT's official distributor in Spain.

See pictures of the installation on Infaimon’s blog (in Spanish)