Home Game: AVT exhibits at Vision China 2013 in Shanghai

Allied Vision Technologies showcases latest machine vision cameras on new booth from March 19-21, 2013. Shanghai team introduces itself to the Chinese market.

Allied Vision Technologies (AVT) will be exhibiting at the Vision China show from March 19-21 in Shanghai. It is the first participation of the camera manufacturer since it opened an office in Shanghai to serve the Chinese market in October 2012. On a brand new, modern booth, visitors will be able to discover the latest camera highlights of AVT.

Small Twins: AVT Mako Series with GigE Vision and USB3Vision
Highlight of the AVT booth is the Mako. Mako is an ultracompact machine vision camera with a typical 29 x 29 mm format. Two interfaces will be available: GigE Vision with Power over Ethernet or USB3Vision. The GigE version will include seven models with resolutions ranging from VGA to 4.2 Megapixels. The USB3 Vision will be available later this year with five sensors and VGA up to 4 Megapixels resolution. Both variants will feature the latest CMOS sensor technology.

Big is Beautiful: New High-Resolution Prosilica GT Models
Visitors of Vision China can discover the new Prosilica GT high resolution models including the Prosilica GT6600 camera that offers the highest resolution of the AVT portfolio with a 29 Megapixel CCD device from Truesense Imaging.

Manta: Unrivalled flexibility
The Manta camera family offers a very wide choice of CCD and CMOS sensors and options. With 9.2 megapixel resolution in a compact format, the Manta G-917 closes the gap between conventional machine vision cameras and those with very high resolution that use 35mm full format sensors. The Manta G-917 comes equipped with Sony’s newest 1/1“ ICX814 EXview HAD CCD II sensor.

Machine Vision, Human Contact
Vision China will offer Chinese visitors a unique opportunity to get to know their new AVT contact persons in Shanghai and discuss projects and applications with experts from the company’s international Application Engineering team.

Vision China – Booth # W1.1218

March 19-21, 2013
Shanghai New International Expo Center