Allied Vision's Alvium Camera Series nominated for Embedded Award 2019

New camera series proposed for the Embedded Award in the Embedded Vision category at Embedded World

Allied Vision's revolutionary camera series for Industrial Embedded Vision has been nominated for the Embedded Award in the Embedded Vision category. A jury of industry experts selected the innovative camera module, powered by the ALVIUM® technology developed by Allied Vision, for the nomination.

The prize will be awarded at the Embedded World Exhibition & Conference 2019 in Nuremberg in February. The nominated Alvium camera series will be the focus of Allied Vision's presence at the leading international trade fair for embedded systems from February 26th to 28th 2019 (Hall 3A, booth #418).


Machine Vision performance for embedded systems

The Alvium Camera Series is an innovative camera platform that combines the advantages of classic machine vision cameras with the advantages of embedded sensor modules: extensive functions for image correction and optimization, a large selection of state-of-the-art sensors, intelligent power management, cost-optimized design, and a small form factor with modular concept.

ALVIUM® technology, an Application-Specific Integrated Circuit (ASIC) with integrated image sensor processor (IPS) and image processing library (IPL) ), delivers industrial performance to embedded vision. By shifting image correction and processing tasks from the host to the camera’s ALVIUM® IPL, engineers can offload the CPU on their embedded boards for alternative processing tasks or reduce overall system cost by downsizing their host processor.


Live demonstrations

From the presentation of the various camera models, the selection of compatible embedded boards and available interfaces to the optimal software connection, visitors will receive comprehensive information about the versatile possibilities of the new embedded camera module. Several live demonstrations running on different embedded boards show cameras of the Alvium Series in action. Additionally, Allied Vision cameras and live demos are shown at the following booths:

  • Antmicro Ltd.: Hall 4A, Booth #621
  • NXP Semiconductors Germany GmbH: Hall 4A, Booth #220
  • Toradex AG: Hall 4, Booth #410


In brief

  • Embedded World Exhibition 2019
    February 26-28, 2019
    Nuremberg Exhibition Center
    Allied Vision booth: Hall 3A, Booth 418
  • Allied Visions presentations at the Embedded World Conference 2019

    "High Image Quality for Embedded Vision Applications"Henning Haider
    February 26, 2019, from 11:30 AM - 12:00 PM

    "Bridging Embedded Vision and Machine Vision with a Hybrid Driver"
    Mark Schenk, Sebastian Günther
    February 26, 2019, from 5:00 PM - 5:30 PM