Allied Vision will participate in the Vision China (Shanghai) 2021 at Shanghai New International EXPO Center from 17th to 19th Mar, 2021 (Hall W1, booth No. 1100). The company has a joint booth along with its sister companies from TKH Vision group, covering a wide selection of vision camera portfolios and will demonstrate the latest vision technology to visitors.
During the exhibition, Allied Vision will showcase several new machine vision camera models of the Alvium 1800 U , high-resolution Prosilica GT, and Goldeye shortwave infrared camera series. Visitors can discover almost all types of camera portfolios to fulfill their application needs, from VGA to high resolution and from visible light to shortwave infrared. Our technical experts will hold 2 onsite product workshops each day at the booth, both in the morning and afternoon.
Embedded Vision Cameras
Embedded vision is one of the most popular vision technology trends in recent years. The Allied Vision Alvium 1500 C and 1800 C camera series are innovative camera platforms that address the limitations associated with current camera and sensor modules for embedded applications and offer system designers a previously unknown level of freedom. Powered by the revolutionary ALVIUM Technology, a unique system-on-chip designed by Allied Vision, Alvium cameras deliver industrial performance to embedded vision.
During the show, visitors will receive comprehensive information about the versatile possibilities of the new embedded camera module. Along with Intelligence Imagine, our local partner, a live demonstration using an Alvium 1800 C board level camera to build an intelligent camera system will be provided.
PC based Machine Vision Cameras
With over 32 years of expertise in machine vision solutions, Allied Vision has a broad range of machine vision camera products to meet different needs from customers. Being the flagship product from Allied Vision, Alvium 1800 U cameras provide high-performance imaging with ALVIUM® Technology for industrial applications. Alvium cameras are extremely small and power-efficient, while at the same time deliver high image quality and frame rates at an affordable price. With its USB3-Vision-compliant interface and industrial-grade hardware, it is an ideal choice for different machine vision applications. Furthermore, Allied Vision will release 5GigE version of Alvium cameras for customers who are looking for upgrading current GigE cameras to higher bandwidth/resolution cameras. Conventional GigE models such as Mako/Manta series will also be demonstrated at the booth.
SWIR Imaging
In addition to visible light cameras, also Goldeye short wave infrared (SWIR)camera will be demonstrated during the show. Comparing to visible light cameras, SWIR cameras can detect invisible light (typically between 900-1,700nm) and are widely used in scientific research, semiconductor inspection and spectral imaging (e.g. material analysis) applications .
As one of the market leaders in SWIR imaging, Allied Vision will demonstrate the first time the new Goldeye models with Sony's innovative SenSWIR sensor technology. . The new VGA (IMX991) and SXGA (IMX990) resolution InGaAs sensors achieve a quantum leap in pixel size (only 5 µm) and image homogeneity through their innovative pixel architecture. At the same time, they enable image acquisition in the visible and shortwave infrared range (400 nm to 1700 nm) with high quantum efficiency. This innovative sensor technology now significantly expands the application possibilities of Goldeye SWIR cameras in terms of spectral analysis of objects and more precise detection of details!
TKH Vision Group
As a member of TKH Vision Group, Allied Vision will share a common space with other sister companies from TKH Vision . Visitors can discover many more exciting products, including line scan cameras, ultra-high-speed cameras and 100+MP high resolution cameras from Chromasens, Mikrotron and SVS Vistek.
Exhibition Details:
• VISION China Shanghai
17th – 19th Mar, 2021
Shanghai New International EXPO Center
• Allied Vision Booth
Hall W1, #1100
• Allied Vision workshop at the booth, with lucky draw
17th – 18th Mar, 2021 (2 days, 2 sessions per day in the morning and afternoon)
10:30 ~ 11:00 “Alvium Camera Series”
14:00 ~ 14:30 “Goldeye SWIR Camera Series”
• CMVU Machine Vision and Industrial Application Conference
Allied Vision Session
“ The Appication, Trend and Development of Embedded Vision“
Date&Time:17th Mar, 2021,15:30 - 16:00
Conference Area