Bonito - shortest exposure time

To set the minimum exposure time of 0.0015 ms with DeviceConfig, follow this instruction:
-  Tab: Timer & Hardware Parameters
- Exp Timing Mode set to Image On Demand (IOD) with Exposure Timer & FDT (M=03)
- Prescaler value set to 83 (K=0053)
- Exposure Time [ms] set to 0.0015 (E=00000001)

 

Note: There are two prescaler values (Granularity) to be mentioned without adding jitter to the exposure time:
- 83 (0x53) to enable the shortest possible exposure time (not the smallest available value)
- 167 (0xA7) to enable the longest useful exposure time.



Zurück zur Übersicht