Universal Package logging and troubleshooting (UniAPI, UniControl)

Logging:

In order to write all calls and return codes to UniControl.log (for example, C:\WINDOWS\system32), copy the UniControl.ini file into the directory where UniControl.dll is loaded.

Since the logging decreases the performance, use it only for debugging.

Troubleshooting:

UniAPI supports AVT cameras loading interface-specific core libraries. For troubleshooting the camera behavior, these APIs and viewer applications could be helpful:

Interface

API

Viewer

Package

1394 DCAM

FireGrab

GrabDemo.exe

FirePackage

GigE Vision

PvAPI

SampleViewer.exe

GigE Sample Viewer

 



Zurück zur Übersicht