Allied Vision Technologies Asia to Exhibit at NEPCON Vietnam 2012

Allied Vision Technologies Asia, the Singapore-based subsidiary of Allied Vision Technologies, will be exhibiting at the NEPCON Vietnam 2012 in Ho Chi Minh City from October 4th – 6th (booth #L03)

Now in its 4th edition, NEPCON Vietnam 2012 is Vietnam’s Only Exhibition on SMT & testing technologies and supporting industries for electronics manufacturing.

Camera Highlights

AVT will be showcasing a selection of its latest camera models from the Manta family of feature-rich GigE Vision cameras with an outstanding price/performance ratio and many modular options to fit into any applications, the Prosilica GT family of Gigabit Ethernet cameras designed to perform in extreme environments, the fast Prosilica GX that combine high frame rates and high resolution with up to 240 MBytes/s bandwidth, and the Guppy PRO entry-level cameras with IEEE1394b interface.

AVT industrial cameras are ideal for a wide range of demanding applications including machine vision, industrial inspection, automation, medical imaging, scientific research, ITS & traffic monitoring, security, and more.


Allied Vision Technologies Asia Pte Ltd
NEPCON Vietnam 2012
October 4-6th, 2012 - (Booth #L03)
Saigon Exhibition & Convention Centre, Ho Chi Minh City, Vietnam