档案

AVT to showcase CCD, CMOS, high resolution, and infrared cameras at Photonics West 2014

2, 4, 29 Megapixel models and new Goldeye SWIR camera to feature on Booth #124 from February 4-6, 2014

Allied Vision Technologies will be showcasing a selection of high resolution, CCD, CMOS and infrared cameras at the Photonics West show in San Francisco, California from February 4-6, 2014.

Two camera models will make their North American debut: the 2 Megapixel Prosilica GT1917 featuring the 1 inch optical format Truesense KAI-02170 CCD sensor, and the newly redesigned Goldeye, a short-wave infrared camera (SWIR) with sensitivity between 900 and 1,700 nm wavelengths.

Other cameras include the ultra-compact 2 and 4 Megapixel Mako G-223 and the NIR optimized Mako G-419, which respectively feature the CMV2000 and CMV4000 CMOS sensors from CMOSIS, and the 29 Megapixel Prosilica GT6600.

Booth #124
SPIE Photonics West
February 4-6, 2014
Moscone Center, San Francisco, California, USA



About Allied Vision Technologies
Founded in 1989, Allied Vision Technologies GmbH of Germany designs, produces and sells cameras and components for image processing in industrial and life science applications such as industrial automation, medical imaging, traffic monitoring, etc. With innovative products, superior manufacturing quality and a service-driven organization, Allied Vision Technologies is well established as a premier provider of digital camera solutions for machine vision worldwide. Allied Vision Technologies owns subsidiaries in Germany, the USA, Canada, Singapore and China and is represented by distribution partners in more than 30 countries.

About Photonics West
Photonics West is the premier photonics and laser event. With more than 1,225 companies, this exhibition continues to be the flagship event to find the latest products, tools, and applications for your research or business needs.