Bat Files are for CXP(Coaxpress)

Save a picture.bmp with defect pixels. (important please use a BMP file)

Drag and drop the saved picture.bmp on the 'Defpix-Create-standard-treshold.bat' --> a defectpixelmap.txt will be created on you computer.

Drag and drop this defectpixelmap.txt on the upload_defpix2-mapindex2.bat --> the defectpixelmap will be uploaded to the camera as custom defect pixel.

In SVCapture > 2.5.0 you can enable the defect pixel map and mark the defect pixels to show which defect pixels will get corrected.


Note: you can edit the threshold of when a defect pixel gets detected, if you open the 'Defpix-Create-standard-treshold.bat' with notepad and add behind the command '--create_defpix_map 10' for example 10. A Defaultvalue is already considered.